ISP1581的WIN10系统下驱动

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ISP1581的WIN10系统下驱动

1,328 次查看
zj99
Contributor I

很多年之前,利用贵公司的ISP1581开发了基于USB通讯的设备。现在,发现该设备在WIN10系统下无法使用,原因是ISP1581无WIN10的驱动。请问,公司里有开发适用于WIN10的该驱动程序么?或者,有之前改驱动的源代码么?

0 项奖励
回复
3 回复数

1,105 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

The ISP1581 is a very old device that is no longer supported.

Thanks

0 项奖励
回复

1,105 次查看
zj99
Contributor I

谢谢答复。

我知道ISP1581是很多年前的产品,目前已不提供技术支持了。那么,贵公司能提供之前该驱动的源代码么?我现在需要在WIN10下使用。如果可以的话,我自己再想办法重新编译生成。

谢谢!

0 项奖励
回复

1,105 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

Sorry all the information is now obsolete and no available

0 项奖励
回复