IIC busy flag always set after IIC enable as master

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IIC busy flag always set after IIC enable as master

跳至解决方案
1,545 次查看
ppd
Contributor II

Hi,

I hope someone can help me with this issue I am struggling with for the last couple of days.

Hardware: QG8 with 5.6K pull-up resistors on both SCL and SDA.

Software:

void main(void) {
  MCU_init();

  IICC = 0x00;
 
  IICC_MST = 1;
  IICC_IICIE = 1;
  IICC_IICEN = 1;
 
  while(IICS_BUSY) { }
}

Problem:

After line "IICC_IICEN=1" IICS_BUSY is set and never cleared. Is this normal? If so, how can I clear it? If it is not OK then what am I doing wrong?

This happens only if I set the master bit (i.e "IICC_MST = 1"). Currently there is no other device in the system, just my QG8 with it's pull-up resistors.

Thank you!

Paul.

标签 (1)
0 项奖励
回复
1 解答
1,266 次查看
kef
Specialist I
  •  Is this normal?

Yes. You are not just switching slave<->master, setting MST bit generates start condition on the bus. BUSY just tells you if bus is free, = that no master (including your own node) generated start condition, both IIC lines are not driven low. Of course bus is busy when MST is set.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,267 次查看
kef
Specialist I
  •  Is this normal?

Yes. You are not just switching slave<->master, setting MST bit generates start condition on the bus. BUSY just tells you if bus is free, = that no master (including your own node) generated start condition, both IIC lines are not driven low. Of course bus is busy when MST is set.

0 项奖励
回复
1,266 次查看
ppd
Contributor II

Ah, I see...

 

Thank you, kef!

0 项奖励
回复
1,266 次查看
ppd
Contributor II

More info.

 

I also have an interrupt service routine:

 

interrupt 17 void Viic_isr(void){

  IICS_IICIF = 1;
           
}

 

Before the interrupt service routine is called, IICS is 166 (i.e TCF, SRW and IICIF are set). After acknowledging the interrupt IICS reads for one cycle 164 (i.e TCF and SRW are set) after which it becomes 166 again and the process repeats itself.

0 项奖励
回复