IIC Clock stretching on an MC9S08SH8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IIC Clock stretching on an MC9S08SH8

ソリューションへジャンプ
2,000件の閲覧回数
Ingo_Michael
Contributor II

Hello @ All!

 

Does anyone know if the MC9S08SH8 do Clock Stretching automatically (in Hardware), or do I have to implement it in my software routines?

 

Do I have to wait for the ´"IIC Interrupt flag" in IICS (Bit 1) or is it better to wait for the "Transfer complete flag" (Bit 7) in IICS after sending one byte of data to provide clock stretching? Now I am using the interrupt flag.

 

Regards

 

Ingo

ラベル(1)
0 件の賞賛
返信
1 解決策
1,730件の閲覧回数
Ingo_Michael
Contributor II

Problem solved. I had some problems reading a IIC slave device.

 

Thanks!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,731件の閲覧回数
Ingo_Michael
Contributor II

Problem solved. I had some problems reading a IIC slave device.

 

Thanks!

0 件の賞賛
返信