Dear all,
1) Is there an IEC 60730 Class B Safety Library for S08PT60 ?
2) Is it easy to port the IEC 60730 Class B Safety Library from S08PBxx to S08PT60 ?
Thanks,
Regards,
Carl
Hi @CarlLee,
No, there is no IEC 60730 Class B Safety library for S08PT60, also there is no documentation regarding a port from S08PBxx to S08PT60.
A recommendation could be to check the difference between both processor in order to see if a change in the IEC 60730 Class B Safety library is necessary.
An apology for the inconvenience.