IEC 60730 Class B Safety Library for S08PT60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC 60730 Class B Safety Library for S08PT60

144 Views
CarlLee
Contributor III

Dear all,

1) Is there an IEC 60730 Class B Safety Library for S08PT60 ?

2) Is it easy to port the IEC 60730 Class B Safety Library from S08PBxx to S08PT60 ?

Thanks,

Regards,

Carl

Tags (1)
0 Kudos
1 Reply

101 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @CarlLee,
No, there is no IEC 60730 Class B Safety library for S08PT60, also there is no documentation regarding a port from S08PBxx to S08PT60.
A recommendation could be to check the difference between both processor in order to see if a change in the IEC 60730 Class B Safety library is necessary.

An apology for the inconvenience.

0 Kudos