ICS protection against loss of lock an loss of clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICS protection against loss of lock an loss of clock

1,006 Views
matri
Contributor I

Hello,

I'm currently using a QE8 microcontroller in my application. The ICS module is designed for lower power operation and has no features that allow monitoring of loss of lock or loss of clock. I read  AN3499, on paragraph 2.1.7, in the event of loss of lock, the ICS attempts to regain FLL on its own. I have doubt on this sentence, it means that the microcontroller change it mode of operation and come in default mode, FEI, if a loss of lock occur?

 

The ICS module contains an indipendent clock source for the COP watchdog timer that can rest the MCU if the CPU and bus clocks are corrupted. I suppose to enable the COP watchdog and use for it the indipendent clock source (1KHz clock), if a loss of clock occur, betwen this event and the COP reset the MCU, the bus frequency falls to 0Hz?

 

Thanks in advance.

 

Marilena

Labels (1)
0 Kudos
Reply
1 Reply

652 Views
bigmac
Specialist III

Hello Marilena,

 

Do you have an experience where the FLL did not attempt to regain lock?

 

The ICS should continue in the currently selected mode, unless there is a reset.  Using the internal reference, any loss of lock will be temporary, maybe due to a step in Vdd voltage.  I can't think of any other causes.

 

Using an external reference, loss of this reference, for any reason, would cause loss of lock and loss of clock.  However, a reset would need to occur to revert to FEI mode.  Under these circumstances, using the independent COP clock source would eventually result in a reset, as you suppose.

 

Regards,

Mac

.

0 Kudos
Reply