bigmac wrote:
Hello,
When the factory calibration is done, this will occur at a specific, but unspecified, ambient temperature and supply voltage. These conditions may no longer exactly apply for your application, particularly with the supply voltage. Additionally, it is possible that variations in the device mounting on the circuit board will affect stray capacitance, and therefore may also have some affect the calibration of the internal reference frequency.
These factors may result in the "initial accuracy" of the calibration to be somewhat outside the specified limits. The use of the factory determined trim value will typically ensure that the baud rate for SCI serial communications will have sufficient accuracy.
What accuracy do you actually need to achieve for your application? I would strongly recommend that the trim value be recalibrated when the firmware is programmed, to achieve the best initial accuracy.
Regards,
Mac
This question is not for any application...yet 
I'm just comparing different microcontrollers (AVR, PIC, 78K...etc)
Most likely the MCU would be recalibrated during programming, as you suggested.
But I wanted to know what accuracy one can expect over the whole voltage and temperature ranges when fresh out from the Freescale factory.
Do I interpret you answer correct, if think you mean that the Freescale factory trim is not within the +/- 2%?
But most likely not much higher?!