I2C Issue with MC9S08AC128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C Issue with MC9S08AC128

5,175件の閲覧回数
preetuabraham
Contributor III

Hi,

I ma facing issue for I2C interrupt not getting hit even after initializing the registers. Even the initialization to F0 does not get set initially.

Since I am transferring multiple data at a time later It gets set to FO

Snippet in main file:

I2C initialization

/* Initialize the I2C Module. */

_IIC1A.IIC1AData = 0x02; /* Set the master address to be 1 */

_IIC1F.IIC1FData = 0x06; for Bus frequency of 6.75MHZ

YYY[][] AND XXX[][] are initialized to set of values and then initialized as below

/* configure 1 */

for (i = 0; i < YY; i++)

{

SendI2CData(&YYY[i][0]);

 

for (j = 0; j < XX; j++)

{

SendI2CData(&XXX[j][0]);

/* Initialize ourselves as the master by setting IICEN, IICIE, MST and TX. **

/*within SendI2CData*/

_IIC1C1.IIC1CData = 0xf0;

Snippet for interrupt

__interrupt void __near _Iic_Isr(void) {

/* Declarations and Initializations. */

volatile Uint8 DummyRead;

/* Statements. */

/* Clear the Interrupt Pending flag. */

_IIC1S.Bit.iicif = true;

/* Check the mode of operation; are we master. */

if (_IIC1C1.Bit.mst) {

/* We in Transmit mode. */

if (_IIC1C1.Bit.tx) {

/* Have all the bytes

 

0 件の賞賛
返信
10 返答(返信)

4,880件の閲覧回数
mfugere
Contributor III

Have you tried setting the IICEN, MST, TX bits within your IIC initialize routine (which is where I would put it anyway), and just set the IICIE bit within your SendI2CData() function?

Are you certain that your slave/target device is connected and able to generate the ACK bit on the end of the transfer?

0 件の賞賛
返信

4,880件の閲覧回数
mfugere
Contributor III

Also, are your linker file, and interrupt vector source files setup to put the address of your IIC_ISR() function at the IIC1 vector address location at flash memory location 0xFFC6:FFC7?   The address of your ISR must be loaded at the proper vector table location to be called when the IIC1 interrupt occurs.

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

Hi Michael,

I will explain clearly what I am observing

So after initializing IIC1A,IIC1f,IIC1C1 to desired values. When trying to set in SendI2CData()  the IIC1C1 to 0xF0,it takes 0xD0 and it shows IIC1S as 0x92.After this its goes to IIC ISR but it does not transfer since the master bit is not set. Again SendI2CData()  is called to transfer the next set of data, this time it sets IIC1C1 to 0xF0,IIC1S shows 0x80 but it does not enter the IIC ISR routine again

0 件の賞賛
返信

4,880件の閲覧回数
mfugere
Contributor III

At the moment I am not sure what might cause the behavior you describe - the master mode bit should remain set if you are setting it.  Maybe try to set the master bit first in the initialization routine, then OR in the enable bit and set that too?   I have seen some peripherals on some micros not initialize properly depending on the sequence of configuration bits, but I have not seen this behavior with this series (9S08AC) of devices.

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

I think there is some I2C register settings issue with HCSO8 . I checked whether the SCL and SDA line connected to different units were connected and it shows all are connected..

Something is not making the bits to set even though it is R/W register

0 件の賞賛
返信

4,880件の閲覧回数
mfugere
Contributor III

This does appear to be a bit odd.   I've used I2C on many microcontrollers before, but my recent project (involving (2)  MC9S08AC60) used SPI interface instead due to legacy requirements, so I don't have ready code on hand for I2C to share that I know for certain is working on MC9S08AC chips.

Have you looked at this I2C application note for any clues?

http://www.nxp.com/assets/documents/data/en/application-notes/AN3291.pdf

Have you made any progress?

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

Yes Michael,

 it behaves weird .I had done some combinations to make  that it set and it was working yesterday by getting the bit to set . But today with same code it is behaving again like that .Any suggestions to avoid this

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

I am setting 0xf0 in IIC1C1 register and it is setting as 0xd0

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

Thanks Michael for the reply

Yes the interrupt is placed at FFC6 location as per the project prm file

The problem I am facing is .mst bit is not getting set and it shows IIC1S that there is an arbitration loss bit getting set

If I am giving 0xFO it is taking as 0xD0

0 件の賞賛
返信

4,880件の閲覧回数
preetuabraham
Contributor III

I am initializing 0xf0 in IIC1C register and it is setting as 0xd0

0 件の賞賛
返信