I meet a strange question of MC9S08AW60 CFUE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I meet a strange question of MC9S08AW60 CFUE

616件の閲覧回数
wangbaode
Contributor IV

Hi,

There is a strange question,when i program MC9S08AW60 CFUE.

I program a mass of MC9S08AW60 CFUE chip with USBDM.but only one chip has the question as follow.

I have two programs .program2 can be programed with no error.But program1 meet the question.

6439_6439.pngpastedImage_0.png

program2 is larger than program1.

So i'm confused.

ラベル(1)
タグ(2)
0 件の賞賛
3 返答(返信)

415件の閲覧回数
bigmac
Specialist III

Hello,

If this is occurring for a single device only, maybe this device is faulty.  I would assume that attempting to program an improperly erased device may cause this error.

Regards,

Mac

0 件の賞賛

415件の閲覧回数
wangbaode
Contributor IV

Hello,

I find the reason .I chose chip type as MC9S08AW32 when i new a project. so to program some chips is ok and to program some chips is error.when i set chip type as MC9S08AW60,it's ok.

0 件の賞賛

415件の閲覧回数
weapon
Senior Contributor I

Hi Baode,

I haven't ever used USBBDM, I recommend you to raise this question to USBBDM's vendor.

If you use PE USBMultilink, I may provide some help. Hope you understand.

0 件の賞賛