How long is the recovery time of MC9RS08KA4 from stop mode to run mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How long is the recovery time of MC9RS08KA4 from stop mode to run mode?

ソリューションへジャンプ
1,029件の閲覧回数
wangbaode
Contributor IV

How long is the recovery time of MC9RS08KA4 from stop mode to run mode?

In datasheet , I can't find the description.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
930件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

Hi

based on the datasheet point 3.11 page 21, typical wakeup time from Stop is

 

t_wakeup = 100us if IREFSTEN =0 or

t_wakeup =  86us if IREFSTEN = 1

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
931件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

Hi

based on the datasheet point 3.11 page 21, typical wakeup time from Stop is

 

t_wakeup = 100us if IREFSTEN =0 or

t_wakeup =  86us if IREFSTEN = 1

Pavel

0 件の賞賛
返信