How can i use internal flash memory in JM60 for MSD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i use internal flash memory in JM60 for MSD?

2,211件の閲覧回数
eduardo1
Contributor II

HELLO,

It's possible to implement a project in MC9S08JM60 to use as a MSD with internal flash memory? How can i do this?

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,125件の閲覧回数
tonyp
Senior Contributor II

Does MSD stand for Mass Storage Device?

If so, yes, in theory.  In practice, no.  With 60K to host you application and storage you can no longer call it 'Mass', can you?

Look at AN3927

0 件の賞賛
返信

2,125件の閲覧回数
eduardo1
Contributor II

Yes, my mistake haha. I need to push some text file like a usb stick, read into the memory and erase file. Thanks for share the AN, i will read about it.

0 件の賞賛
返信