How can i be sure ICG is Off in Stop mode 3 ? - MC9S08AW16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i be sure ICG is Off in Stop mode 3 ? - MC9S08AW16

1,799件の閲覧回数
PatrickP
Contributor I
Hello,

I use a MC9S08AW16 with a battery and programmed it with BDM.
My program use Stop mode 3. I want to be sure that the ICG is OFF. (ENBDM in BDCSCR is 0).

If i correctly understand the datasheet, if BDM is plug when MC9S08AW16  turn on, ICG is on.

But when i unplug BDM do ICG be off or do i need to realize a reset on the MC9S08AW ?

Best regards,

Patrick
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-10-03 07:07 AM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

940件の閲覧回数
PatrickP
Contributor I
Thanks a lot !

Patrick
0 件の賞賛
返信

940件の閲覧回数
BasePointer
Contributor II
After unplug the BDM pod, you need a reset to disable ENBDM.
0 件の賞賛
返信