Hi people...i tried to find any kind of simple interface... MC9S08QE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi people...i tried to find any kind of simple interface... MC9S08QE

3,531 Views
jlflorio
Contributor I
Hi people...i tried to find any kind of simple interface between S08QE (3V) and LCD Module (5V)but nothing. Can you tell me about any AN or circuits?
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-01-29 03:28 PM
Labels (1)
0 Kudos
Reply
5 Replies

1,619 Views
erooll
Contributor II
Hi... I ever use this simple circuit to interface from 3V out to 5V in

fast diode 4148
resistor 10K


                                                      
0 Kudos
Reply

1,619 Views
peg
Senior Contributor IV
Hello and welcome to the forums jlflorio,

It's all here in the forums you just need to learn how to use the search facility here (or even use google, restricted to this site).

This previous post by me seems to answer your query exactly.

0 Kudos
Reply

1,619 Views
RickN
Contributor I
Hi,
 
   Have you considered the 9S08LC60?  It has support for a segment based LCD. 
 
   Just a thought,
 
    Rick
0 Kudos
Reply

1,619 Views
bigmac
Specialist III
Hello,
 
If you are using one of the common alphanumeric LCD modules, with either 4- or 8-bit interface modes, I suggest you check its specification for digital input switching level.  You may find that a 3.3 volt swing from the MCU is adequate, even though the LCD operates from 5 volts.  To avoid any possibility of return data from the display, and a voltage mismatch, you would need to set the WE pin for continuous write mode.
 
Regards,
Mac
 
0 Kudos
Reply

1,619 Views
mke_et
Contributor IV
Well, what kind of LCD? Graphics array? 1-line? 2-line? 4-line? 640x480?

There's a lot out there.

But if you're looking for something simple, you STILL have to pick your LCD first. If you want something just to display a line or two of text at 16 or so characters, there's simple 4-bit interfaces. I've seen 4-line with 40 characters that still can use a simple 4-bit interface.
0 Kudos
Reply