Hi         MC9S08GB60  -  I have one more problem for that i want sollu...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi         MC9S08GB60  -  I have one more problem for that i want sollu...

1,288件の閲覧回数
santhu
Contributor I
Hi   
    
 I have one more problem for that i want sollution from your side. I'm using MC9S08GB60 controller of HCS08 family.I use USB MULTILINK for debugging my code. While debugging my code in the command window the frequency changed from 4MHz to 0Hz. After that one more diologue box (Power cycle diologue) saying that "Under 0.1V,turn MCU power ON and then click ok.This will attempt to enter debug mode through power on reset sequence (BKGD currently is driven low)".What this statement means.can u suggest me on this
  
 During this time in my target board the voltage between BKGD and GND was high (3.3V).Suggest me on this issue.
 
With regards
         santhu   
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-07-14 08:37 AM
ラベル(1)
0 件の賞賛
返信
1 返信

653件の閲覧回数
Ake
Contributor III
Hi there,
It looks like you have managed to turn the oscillator off to the 9S08GB60.
If you burn a new program into the MCU, and then single-step the code,
 
If it is possible,  then continue single stepping the code until you loose control.
I would guess it would be in the setting of the ICG.
 
If it is not possible, the CodeWarrior immedieatly complains about lost frequency, I would check that I have selected the right MCU.
If you click on the "Change MCU/Connection...." box on the main screen. Check that you have the right MCU selected.
 
Regards,
Ake
0 件の賞賛
返信