Hello, I need to find eagle library for microcontroller M... - MC9S08LC60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hello, I need to find eagle library for microcontroller M... - MC9S08LC60

跳至解决方案
3,951 次查看
Jura
Contributor I
Hello, I need to find eagle library for microcontroller MC9S08LC60 package 64-Pin LQFP and 80-pin LQFP. Thanks for help! Jiri
 
 
 
 
 
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-06-13 08:17 AM
标签 (1)
0 项奖励
回复
1 解答
890 次查看
protoease
Contributor II
You could just make one, its fairly easy to do- start by making a symbol for each type, 64 and 80 pin.  Then you can just copy in the package from the smd-ipc family and map the symbol pins to the footprint pins.

I can help you make a library part for this part if you want.  I've made my own library that so far contains the QG, QE, JM, AW/AC.  Will continue to add to it and make it available to everyone if desired.


Aaron

在原帖中查看解决方案

0 项奖励
回复
1 回复
891 次查看
protoease
Contributor II
You could just make one, its fairly easy to do- start by making a symbol for each type, 64 and 80 pin.  Then you can just copy in the package from the smd-ipc family and map the symbol pins to the footprint pins.

I can help you make a library part for this part if you want.  I've made my own library that so far contains the QG, QE, JM, AW/AC.  Will continue to add to it and make it available to everyone if desired.


Aaron
0 项奖励
回复