Hello Diode
I know this is a long past issue, but in light of a number of your facts, flags go up for me, consideringm a problem we are having with the GT16 we are using.
1.The RESET pin sitting at near VCC/2
2. your comment about thinking that your .1uF cap was actualy a resistor
3. removing the cap fixes the problem
4. problem doesn't show up for a number of months
A couple of questions first;
Did you use no-clean or flux core solder?
Do you conformally coat you product?
Here are my thoughts;
Even though there is an errata on a RESET problem for this family of CPU, the VCC/2 level on the RESET pin may be the key. The residues left by flux and the soldering process, if not cleaned off completely can, over time, and when combined with moisture, cause electromigration; dendrites will grow from one terminal of a biased component (especially caps) to the other, effectively putting a "resistor" in parallel with or even shorting the cap. This proplem can take many months to show up. Since your board is SMD, it is often easy to leave this residue under the component, even after cleaning. This would answer items 1 & 2 above.
If the board is conformally coated, moisture takes more time to accumulate due to the conformal coating and its porosity. The residue consists of weak organic acids which when mixed with water become ions. The process of electromigration requires the ions to grow dendrites. This answers item 4 above. The acids are nomally eliminated by heat, 150 C, which make the resude inert, no dendrite growth possible.
Removing the cap and then putting it or another back would eliminate the dendrite. That would answer item 3 above.
Do a web search for the company Foresight, inc. at www.Residues.com for more information of "dirty" boards. It is fancinating stuff which we are currently dealing with.
Drop me an email at wgreenwald@sloanvalve.com to talk more.
Bill