HC908GR16 -32  and HC908GZ16 -32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC908GR16 -32  and HC908GZ16 -32

1,918 Views
mbandini
Contributor I
What's the differents beetwin HC908GR16 -32  and HC908GZ16 -32
 
And why I can't find GZ16 32 all over the world?
Labels (1)
0 Kudos
Reply
3 Replies

916 Views
mbandini
Contributor I
So if I dont'use msCAN bus
 
But I use a external Oscillator with 16MHz TTL output
 
I can Use GR16 32 pin, they are pin to pin compatible isn't it?
 
I need to Recompile the firmware or not?
0 Kudos
Reply

916 Views
Alban
Senior Contributor II
Hello,

You don't say which one you use now. So can't tell you much.
External square wave of 16MHz will work on all mentioned.

Comparing the pinout, register map, and errata published is the best way for you to assess drop-in replacement.

Alban.
0 Kudos
Reply

916 Views
Alban
Senior Contributor II
Hello,
 
GR should not have a msCAN module and low frequency oscillator (32kHz XTAL typ.)
GRxxA should not have a msCAN module and high frequency oscillator (>1MHz XTAL)
GZ have a msCAN module and high frequency oscillator (>1MHz XTAL)
 
They are all available and shipped around the world. (except countries with an embargo, that goes without saying).
 
Alban.
0 Kudos
Reply