General purpose I/O voltage level problem - Added p/n MC1321x zigbee

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

General purpose I/O voltage level problem - Added p/n MC1321x zigbee

1,535 次查看
bitasobhani
Contributor III
Hi all
I am working on MC1321x zigbee  wireless network.
I need more general purpose I/O than what is available on the board.
I used 74LS374 for adding more I/O ports.
The problem is that 74LS374 uses 5Volt Vcc. However its high output voltage is measured about 3.8Volt which is not too larger than 3Volt(high voltage level of the board). Can I connect this 3.8Volt directly to an input general purpose port of the board or I have to convert it to 3Volt. If so, how can I do that?
Thanks alot 


Message Edited by NLFSJ on 2008-10-13 12:59 PM
标签 (1)
0 项奖励
回复
1 回复

768 次查看
bigmac
Specialist III
Hello,
 
Is there any reason that you can't use a 74HC374 device?  This can operate from a 3 volt supply, and so would be compatible with the MC1321x device.
 
An alternative approach to providing input or output expansion would be to use shift register devices, and to bit bang the SPI communications.  For input expansion, a suitable device might be the 74HC589 or 74HC597.  Multiple devices may be cascaded.
 
Regards,
Mac
 


Message Edited by bigmac on 2008-10-14 03:31 AM
0 项奖励
回复