FBI Mode of MC9S08DZ60

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FBI Mode of MC9S08DZ60

1,289 次查看
Botchico
Contributor I

Hi guy's

 

I am trying to switch my MC9S08DZ60 from the default reset operation mode FEI to the FBI mode.

Therefore I setup the following code:

 

  MCGC2 = 0x00;  /* Set BDIV to 0 -> Divide by 1 */  MCGC1 |= 0x03; /* Enable Internal Reference Clock and let them stay enabled in Stop mode  MCGC1 |= 0x40; /* Select Clock source: Internal Reference Clock */     while((MCGSC&0x0C)!=0x04);   /* Wait until Internal Reference Clock is selected */

 After the command:

 

MCGC1 |= 0x40

the program flow will be frozen, and all displayed data in the debugger will be invalid.

 

Have anybody an idea? What I did wrong?

标签 (1)
0 项奖励
回复
1 回复

748 次查看
pgo
Senior Contributor V

Dear Botchico,

 

Some comments on your code:

- The check for FLL lock appears incorrect. Are you trying to check the LOCK bit?

- The clock shouln't be programmed for /1 bus speed unless the internal clock has been trimmed first.  The clock might be fast and result in an out-of-spec bus speed and lock up the chip.

 

Another possibility is that the BDM you are using can't handle the higher bus frequency after the clock change.


I'm too lazy to check the magic numbers in your code :smileyhappy:  The following is the code I use to  achieve the same thing I believe. You are welcome to try it an see what results you get.

 

 

typedef unsigned char U8;// Clock Trim values in Flash - dummy values overwritten by flash programmerstatic const volatile U8 NV_FTRIM_INIT  @0x0000FFAE = 0xFF;  // LSBstatic const volatile U8 NV_MCGTRM_INIT @0x0000FFAF = 0xFF;  // MSBvoid initClock( void ) {   SOPT1  = SOPT1_STOPE_MASK;  // Watchdog off, STOP enabled, BKGD pin enabled
      if (NV_MCGTRM_INIT != 0xFF) {   //  Only trim & update clock if Trim values have been programmed to Flash.   //  Enabling x1 clock div. on untrimmed device may be out of bus clock spec.
     MCGSC       = NV_FTRIM_INIT;    // Trim the internal clock     MCGTRM      = NV_MCGTRM_INIT;     // Set 16 MHz bus clock assuming 31.25 MHz trim     MCGC2 = (0<<MCGC2_BDIV_BITNUM);
                   // BDIV=0,RANGE=0,HGO=0,LP=0,EREFS=0,ERCLKEN=0,EREFSTEN=0     MCGC1 = (0<<MCGC1_CLKS_BITNUM)|MCGC1_IREFS_MASK; 
         // CLKS=00,RDIV=0,IREFS=1,IRCLKEN=0,IREFSTEN=0    
     // Following only applies for S08MCGV2 (and is default anyway!)     MCGT  = MCGT_DRST_DRS_MASK; // MCGT_DRST_DRS=1, MCGT_DMX32=0           // Wait for FLL lock     while(MCGSC_LOCK == 0) {     }   }}

 

 bye


 

0 项奖励
回复