Example code for internal ADC of MC9S08DZ96

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example code for internal ADC of MC9S08DZ96

2,373 次查看
admin
Specialist II

I am evaluating MC9S08DZ96 for one of the application and interested in testing ADC performance before making decision on ADC and controller. I have evaluation kit with me, is there sample code for internal ADC of MC9S08DZ96, which can be used for basic evaluation testing purpose??

 

Thanks in Advance

Manoj

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

1,237 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport


You can download the dz60_demo.zip from the following link:

http://www.axman.com/content/demo9s08dz60

Also you can check the samples that are install with CodeWarrior the normal folder is

C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\(CodeWarrior_Examples)\HCS08\Evaluation Board Examples\EVB9S08DZ60\C
These samples are for the Evaluation board but you can check the initialization and use it for the DEMO, I believe that the two board has the same package.
On this folder you can find a sample for CAN, LIN, SCI and the demo that use the ADC.

Best Regards,

Jennie

0 项奖励
回复

1,237 次查看
GMVS
Contributor III

hello

did you find anything useful?

i'm in the same situation...

regards

0 项奖励
回复