Does MC9S08PA8 analog comparator have internal protection diodes?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MC9S08PA8 analog comparator have internal protection diodes?

ソリューションへジャンプ
1,187件の閲覧回数
MAPC
Senior Contributor I

Hello,

 

I'd like to know if MC9S08PA8 analog comparator has internal protection diodes. The reference manual doesn't bring this information. Could anybody from NXP answer me this question please?

 

Thanks,

 

Marco Coelho

Applications Engineer

Siletec Eletronica

ラベル(1)
0 件の賞賛
返信
1 解決策
978件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Marco

All functional non-supply pins, except for PTA2 and PTA3, are internally clamped to VSS and VDD,

This also true to the pins with the analog comparator function

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
979件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Marco

All functional non-supply pins, except for PTA2 and PTA3, are internally clamped to VSS and VDD,

This also true to the pins with the analog comparator function

0 件の賞賛
返信
978件の閲覧回数
MAPC
Senior Contributor I

Thank you, Pedro!

0 件の賞賛
返信
978件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Marco,

The thread is under CodeWarrior Community box.

I will move it to hardware team box.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信