Does CodeWarrior 11 support MC9S08SG8?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does CodeWarrior 11 support MC9S08SG8?

跳至解决方案
2,943 次查看
w_lingjun
Contributor III

Hi,

When I new a bare board project in CodeWarrior 11, I can't find this MCU: MC9S08SG8 on devices interface.

So does CodeWarrior 11 support MC9S08SG8?

Best regards,

Sarah

0 项奖励
回复
1 解答
2,927 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,940 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Yes

 

vicentegomez_0-1607348148178.png

You should have it.

 

Regards

Vicente G

0 项奖励
回复
2,934 次查看
w_lingjun
Contributor III

Hi Vicente,

Thanks for your reply.

This is my CW  version page

cw11_version.png

And this is the devices select interface when new a project, there is no HCS08SG Familly.

cw11_1.png

And I and can't search any devices when input MC9S0.

cw11_0.png

Is there any update packages should I install?

 

Best regards,

Sarah

 

0 项奖励
回复
2,928 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I believe that the problem was on the installation, you do not have installed the S08 family, the easier solution is to reinstall Codewarrior and when you are installing it you need to select the S08 devices.

I hope this will help you

0 项奖励
回复
2,898 次查看
w_lingjun
Contributor III

Hi Vicente,

Thank you very much!

Sorry for replying so late. I just installed S12Z family when I did some work on MC9S12ZVML128. It is too big to install all family~

Beat regards,

Sarah

 

0 项奖励
回复