Hello all. I'm trying to read an analog input ranging from 0 to 2.5 volts, convert it to a digital signal, and read the bits outputted through hyperterminal (for now...). I will eventually be using a gui to take these bits and make sense of them but just want to get a solid reading first. I am getting a reading but it is a bunch of letters and symbols on hyperterminal and I'm not sure why. When I remove my input I get a bunch of "]"'s, so I know it's reading something from the ADC when it's hooked up. Below is my code and a picture of my output. Any ideas would be appreciated. Please let me know if anything should be changed or is unessesary as I'm new to microcontrollers, Thanks!
My hardware/Software:
* DEMOQE128 board
* MC9S08QE128
* Code Warrior
My code:
int PyrRding; void main(void) { /*******Set up SCI Registers********/ SCI1C1=0x40; SCI1C2=0x08; /***********************************/ PTCDD_PTCDD5=1; PTCD_PTCD5=1; SCI1BDL=0x1A;//baud rate=9600bps and bus freq=4MHz. /**********Pyranometer ADC**********/ ADCSC1_ADCO = 1; // enable continuous conversion ADCCFG_MODE = 0x00; // 8 bit mode PTADD = 0x00; // initialize as input /************************************/ /****************First ADC to SCI*************/ for(;;){ ADCSC1_ADCH = 0x00; // set channel PTA0 ADCSC1 = 0; // Commence new conversion Ch0 while (ADCSC1_COCO == 0){} // Wait until conversion complete PyrRding = ADCRL; // output 8bit ADC to PyrRding variable while (SCI1S1_TDRE == 0){}; // Wait for the transmitter to be empty SCI1D = PyrRding; // Stores new data to be transmitted via serial port SCI1S1_TDRE = 0; // Clear flag to send __RESET_WATCHDOG(); } /**********************************************/ }
My output:
Solved! Go to Solution.
Hello,
Sorry about the misleading information. Rich T is absolutely correct on both counts. The following revised code should compile.
byte buffer[4], *p;
...
ADCSC1 = 0; // Commence new conversion Ch0
while (ADCSC1_COCO == 0){} // Wait until conversion complete
conv_ASCII( ADCRL, buffer);
p = buffer;
while (*p) { // Check for null character
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCI1D = *p++; // Write character to SCI
}
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCI1D = ' '; // Separator space
Regards,
Mac
Hi,
Here's a simple idea if you are looking for alternatives...
> I'm trying to read an analog input ranging from 0 to 2.5 volts,
> convert it to a digital signal, and read the bits outputted through
> hyperterminal (for now...).
You can just load StickOS onto the QE and then log into it with Hyper Terminal (9600/8/n) and write a program like:
10 dim a as pin pta0 for analog input
20 while 1 do
30 print a
40 sleep 500 ms
50 endwhile
And then save and run it, and the number of millivolts on pin pta0 will be printed to the Hyper Terminal twice a second. You can then set the program to autorun and it will do that whenever the MCU is powered up.
When I run it, I see my pot (on the DEMOQE board), like:
> run
2133
2132
2135
2133
<Ctrl-C>
STOP at line 40!
>
Press <Ctrl-C> to stop the program (to edit it, debug it, etc.).
If you want downloads of StickOS, for the 51QE128 or 9S08QE128, they are at:
http://www.cpustick.com/downloads.htm
You can find full documentation there, as well.
-- Rich
You are sending a raw byte value to a device which is expecting an ASCII value.
The byte valuereturned from the ADC varies between 0 and 255 decimal or 0 to FF in Hexadecimal. To display the numeral "0" to "9" on hyperterminal you must send the hexadecimal values 30 to 39.
There are lots of ASCII tables on the internet if just google the acronym ASCII or just go to www.asciitable.com
You will probably need to write a conversion routine or use one of the stream formating functions like sprintf to format your data before sending it to the serial port to Hyperterminal.
Good Luck,
Peter House
Hello,
The use of sprintf() to do what you require is somewhat over-kill. Here is a much more compact function to do the binary to ASCII conversion. It uses inline assembly code for fast operation. The numeric ASCII characters are written to the buffer, and null termination also occurs.
void conv_ASCII( byte val, byte *buf)
{
__asm {
LDA val
CLRH
LDX #10 // Divisor
DIV
PSHH // LS digit
CLRH
DIV
PSHH // 2nd digit
LDHX buf
ADD #'0' // Convert to ASCII digit
STA ,X // MS digit
PULA
ADD #'0' // Convert to ASCII digit
STA 1,X
PULA
ADD #'0' // Convert to ASCII digit
STA 2,X // LS digit
CLR 3,X // Null termination
}
}
The function might be used in the following manner -
byte buffer[4];
...
ADCSC1 = 0; // Commence new conversion Ch0
while (ADCSC1_COCO == 0){} // Wait until conversion complete
conv_ASCII( ADCRL, buffer);
while (*buffer) { // Check for null character
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCID = *buffer++; // Write character to SCI
}
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCID = ' '; // Separator space
Regards,
Mac
Hello,
berb_15 wrote:
... I'm assuming I can run that assembly code right in with my standard c++ code?
The code is actually a C function - for the moment I suggest that you stick with C code, rather than C++, for your program.
Regards,
Mac
You might try "SCI1D", assuming you are using UART 1.
Or did you forget the ";" on the preceding line, or forget to include "MC9S08QE128.h"?
If you get really stuck, you can usually right-click on a .c file and select "Preprocess" to see exactly what the compiler is complaining about.
-- Rich
Oh, and *I'm* sorry -- I read your code too fast...
You can't do a "++" on a variable declared like:
byte buffer[4];
Change that to a "byte *buffer;" and make sure it points to allocated memory.
Hello,
Sorry about the misleading information. Rich T is absolutely correct on both counts. The following revised code should compile.
byte buffer[4], *p;
...
ADCSC1 = 0; // Commence new conversion Ch0
while (ADCSC1_COCO == 0){} // Wait until conversion complete
conv_ASCII( ADCRL, buffer);
p = buffer;
while (*p) { // Check for null character
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCI1D = *p++; // Write character to SCI
}
while (SCI1S1_TDRE == 0){}; // Wait for transmit buffer empty
SCI1D = ' '; // Separator space
Regards,
Mac
Hi
berb_15 or you can send me your working code of the program. On my mailtomazvalic20@gmail.com).
Thanke you very much!