Demo QE board and BDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Demo QE board and BDM

2,181 次查看
maverick
Contributor I
Hello,

My question is: can I use the Demo QE board's BDM to program any other S08 or S12X? Or is it limited to flexis microcontrolers.

Thank you in advance.

Mav
标签 (1)
0 项奖励
回复
1 回复

708 次查看
JimDon
Senior Contributor III
Add the 6 pin header, get a 6 pin IDC cable, and you are ready to rock.

It is a a full P&E BDM and will work with CFV1, S08 and S(X)12 boards.

However, do not expect it to supply power to the board. I have been told it is also not as well protected and a USB 12 is - not sure what that means.
0 项奖励
回复