Debugger for OSEK turbo application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugger for OSEK turbo application

1,838件の閲覧回数
tupham
Contributor I
Dear all,
 
I have installed Code Warrior for HC(S)08 v5.1 and OSEK turbo v2.3. I have built sample for HC08GZ60 which is available after installing OSEK turbo. I have followed steps to build that sample application and generate all necessary files in 3 folders: bin, gen, obj. Especially in bin, I have the executable file "sample.hex" and the link file "sample.map". But till now, I don't know what the "debugger" is. Is it Code Warrior v5.1? I can't find how to use the debugger in Code Warrior v5.1 to execute that OSEK application. Please help me.
 
Thanks anyway,
 
Tu Pham.
ラベル(1)
0 件の賞賛
返信
1 返信

765件の閲覧回数
CrasyCat
Specialist III

Hello

What happens if you select Project -> Debug?

This should load code on the target and start the debugger.

CrasyCat

0 件の賞賛
返信