Hi,
The sensor used for this task is the MPXV5100GP which have a measurement pressure range from 0 to 100kPa, but this device is a Gauge pressure sensor, which means that it uses the local atmospheric pressure as its reference pressure, which, if I understand well your comments is around 101kPa, so, starting from this point, the MPXV5100GP can measure up to 100kPa (up to 201kPa in this specific case where its reference point is the ambient pressure of 101kPa).
Let me know if I misunderstood your question.
Regards,
Jose