Communication problem with  DEMO09S08QG8 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Communication problem with  DEMO09S08QG8 board

914 次查看
israel_voli
Contributor I

I got a DEMO09S08QG8 board and I already programmed a M9S08QG8 chip using the integrated USB-to-BDM interface of the board in an external target. Now I want to do the same with a MC9S08SE8CRL chip but there is no communiation with the target when I run the debug mode in CodeWarrior V6.3.

 

My question is, what I need to change in the board configuration? Could it be the 3.3V power of the BDM Port and change it for an external 5v power?? 

 

Thak you.

标签 (1)
0 项奖励
回复
1 回复

643 次查看
peg
Senior Contributor IV

Hello and welcome to the fora,

 

In the interest of making more money this sort of functionality has been disabled.

Refer tohttps://community.freescale.com/message/49272#49272

 

0 项奖励
回复