Clock generation without external parts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Clock generation without external parts

2,327 次查看
WimmerChris
Contributor I
Hello everybody,
 
i've a short question: Which HC08 MCUs like the QT4 or QB8 have an internal oszilatior, so that i can run them with out external parts?
 
 
Thanks for help!
With best regards
 
Christian Wimmer
标签 (1)
0 项奖励
回复
4 回复数

1,325 次查看
peg
Senior Contributor IV
Hi Chris,
 
This document helps:
 
 
The clock type column gives the acronym for the clock module type, from there and from a few checks you should be able to work it out. They don't make it real easy, do they?
 
0 项奖励
回复

1,325 次查看
WimmerChris
Contributor I
Hi Peg,
 
thanks for the overview it's pretty good. But i'm sorry it doesn't help me in my problem because, if you look at the QT4A or the QB4 for example you will see that there is a "OSC" at the clock type. (Both devices have an internal oscillator.) But the JL8 (there is also a "OSC" ) didn't have an internal oscillator.
 
Thanks for your help.
Best regards.
Christian


Message Edited by WimmerChris on 2007-05-09 06:48 PM
0 项奖励
回复

1,325 次查看
peg
Senior Contributor IV
Hi Chris,
 
I know my response was fairly useless. I made in in the vain hope that someone at Freescale would see it and realise that filling these tables with useless, company specific acronyms only serves to keep the $%^&*'s in the marketing department happy and does nothing to assist its users.
 
0 项奖励
回复

1,325 次查看
bigmac
Specialist III
Hello Chris,
 
The HC908 devices that have a trimmable internal oscillator are limited to a few series only - Qx series, EY, GT, but not many others come to mind.  A few other series do have an internal oscillator, but is not accurate or stable with voltage and temperature.
 
Trimmable internal oscillators seem much more prevalent within the various 9S08 series, which are more recent devices.
 
Regards,
Mac
 
0 项奖励
回复