Changing the network depth in MC13213 using beekit.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing the network depth in MC13213 using beekit.

1,395件の閲覧回数
Sandra
Contributor I
Hello,

I need to change the zigbee stack profile 1 using beekit "wireless uart aplication". Freescale Beekit lets to change the properties in the components of the project easily.

1) If I need change the network depth (5 in profile 1) to 10 or 15,  which other properties in bee stack should I change? I suppose that properties as number of routers used for energy scan, maximun incoming reports, maximun broadcast transaction table entries, the maximun neighbor table entries supported for the router and the cordinator... which one should be changed exactly?

2) What is the maximun depth that I can use for the network using MC13213 without have problems "out of allocation space"?

Thanks,

Sandra
ラベル(1)
0 件の賞賛
返信
1 返信

636件の閲覧回数
Mads
Contributor V
Sandra,
 
FIrst of all it is VERY important to understand that changing the depth, max children and max routers will render your solution NON-COMPLIANT and you will not be able to:
1. Connect to certified products
2. Certify a public profile, but only as an MSP.
 
 
you must calculate that the biggest address used by the CSKIP address does not surpase the 16 bit integer used for the address.
 
For changing(increasing) the depth you also change(lower ) the maximum number of children and maximum number of routers.
 
As increasing the depth will lower the size of how many children a router has the memory impact will not be increased.
 
BR,
Mads
0 件の賞賛
返信