Can anybody help me with Cracked MC9S08QG8 Demo Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can anybody help me with Cracked MC9S08QG8 Demo Board

2,895 次查看
admin
Specialist II
Hi
I'm Afraid that I've destroyed my demo kit. Demo Board was working good. Bud when I've connected the BDM interface to another cracked device, the Demo Kit get Cracked too. When I tried to connect the BDM Interface to surely working device I make a sure that the Demo Board is cracked becoase the Debugger call error: "Cannot enter background mode"

http://img442.imageshack.us/my.php?image=problemip2.jpg

And when i touched to the Demo Board, the chip U305 and the rezistor R306 was very hot

http://img96.imageshack.us/my.php?image=mc9s08qg8mv4.jpg

So I would like to try change the U305 chip (In my opinion it is cause problems) bud on the chip is writen C6658Z. Bud when i tried to enter this number to Google.com nothing had been found. So i would like to ask you: Did you now the strict name of chip U305? Or did you now what cause problems? Thank you wery much!

I'am sorry, I now that my english is very poor. :smileyhappy:

Message Edited by Mica on 2007-01-1107:02 PM

标签 (1)
0 项奖励
回复
3 回复数

1,176 次查看
thisobj
Contributor III
Hi Mica,

The document, DEMO9S08QG8UG.pdf (in the development kit) contains a BOM for the board.

U305 -- IC-Switch-Smt -- (DCT8) SN74LVC2G66DCT, Analog Sw,Bilateral,Dual -- Digi-Key 296-13271-1-ND

R306 -- Res-Carb-Smt (0805) 1K Ohm,5% -- Emtek CR10-102J-TR

Frank
0 项奖励
回复

1,176 次查看
celsoken
Contributor V
Dear Frank,

I've got two crancked MC9S08QG8 demo boards and I've checked my documentation and the BOM was supressed. My document is Rev. F and I've checked the only change in rev history was the BOM is supressed.

Could you please send me your old DEMO9S08QG8UG.PDF file so I could fix my boards.

Thanks in advance,

Celso
0 项奖励
回复

1,176 次查看
admin
Specialist II
Thank You!!
0 项奖励
回复