Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?

1,273 Views
alan36alexis
Contributor I

Hello! I have a board of a device that I disarmed that brings a JM60. Investigating the board and the datasheet of the JM60, I saw that it brings a USB card connected to the pins USBDP, USBDN, VDD and VSS, also brings a 6-pin BKGD.

My question is this, is it possible to connect it to a PC directly with a USB cable, which is detected, and load the program with the CodeWarrior? Is it possible to do this without the need of a JTAG or a programming device?

Obviously, the functionality for which the board was manufactured is lost, but that is not the problem ...

Thanks in advance, and know excuse my ignorance in the subject

Labels (1)
0 Kudos
Reply
1 Reply

1,141 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

As I know this is not possible.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply