Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?

1,370件の閲覧回数
alan36alexis
Contributor I

Hello! I have a board of a device that I disarmed that brings a JM60. Investigating the board and the datasheet of the JM60, I saw that it brings a USB card connected to the pins USBDP, USBDN, VDD and VSS, also brings a 6-pin BKGD.

My question is this, is it possible to connect it to a PC directly with a USB cable, which is detected, and load the program with the CodeWarrior? Is it possible to do this without the need of a JTAG or a programming device?

Obviously, the functionality for which the board was manufactured is lost, but that is not the problem ...

Thanks in advance, and know excuse my ignorance in the subject

ラベル(1)
0 件の賞賛
返信
1 返信

1,238件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

As I know this is not possible.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信