Calling Firmware Functions in FXTH87xxDD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Calling Firmware Functions in FXTH87xxDD

1,161 次查看
f20150335
Contributor III

Hi, i cannot get the result in the register when I am multiplying two numbers using the following code - 

pastedImage_1.png

Am I completely incorrect in calling the function. How should it be done?  When i write TPMS_MULT_SIGN_INT16 I get an error message too. So what should I do to call this function?

I am only implementing this function for learning as later I would have to call the read_pressure type functions too.

0 项奖励
回复
0 回复数