Evandrios......
If you are refferring PA as the Power Amplifier Just consider this....
PA is PTD2
RxSwitch is PTD1
TxSwitch is PTD0
On use....... write this values onto the ports:
Tx PA_EN=1 Tx_EN=1 Rx_EN=0
Rx PA_EN=0 Tx_EN=0 Rx_EN=0
Best regards
Marquinho
Sorry on my last post I did a mistake, please consider this....
Tx PA_EN=1 Tx_EN=1 Rx_EN=0
Rx PA_EN=0 Tx_EN=0 Rx_EN=1
My apologies to any cirmcunstances caused....
Best regards
Marco
I have the same problem!
The settings you refer using MAC codebase are into the file NV_DATA.h
/* Energy detect threshold for determining a clear or busy channel during an Energy Detect operation from the MACA */
#define gCcaThreshold_c 0x39
#define gDualPortRFOperation_c TRUE
#define gPowerLevelLock_c FALSE
#define gDefaultPowerLevel_c gAspPowerLevel_3dBm //hex: 0x11
#define gEnableComplementaryPAOutput_c FALSE
#if gTarget_UserDefined
/* User defined tuning values */
#define gXtalCtuneValUserDefined_c 0x04
#define gXtalFTuneValUserDefined_c 0x0E
#endif
The MAC stack drives internally this signals. But with this settings I can't reach the best tx power.