Adding an LCD to a SRB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding an LCD to a SRB

2,047 次查看
flyingasics
Contributor I
We are using the MC13213 EVK (1x NCB 2xSRBs) to design a wireless secuity system for our building.
We will need to add an LCD to the SRBs is this possible w/o adding more circuitry besides the LCD? Or do will we need to add additional driver chips?
 
Thanks
标签 (1)
0 项奖励
回复
2 回复数

886 次查看
addiyi
NXP Employee
NXP Employee
You can use PTB port for connecting a LCD display to SRB board (pins 19 - 26 on J103 connector). NCB board use the same port for connecting LCD display.

Adrian
0 项奖励
回复

886 次查看
JimDon
Senior Contributor III
If you have 6 outputs left, you can use a "standard" 16x2, 20x3 20x4 LCD.
The link shows one from sparkfun. There are very common.
You can also get it with a serial interface if you have a port left.

0 项奖励
回复