Acceptance Mask MC9S08DZ96MLH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Acceptance Mask MC9S08DZ96MLH

696 Views
Mizuz
Contributor II

Hi, I am using the MC9S08DZ96MLH chip in a project. In this project, this chip receives messages with the following identifiers. Considering that this chip is placed on the car's CAN network and many other identifiers are sent on this network, the amount of stimulation of receiving interruptions in the CAN network of this chip is very high, which causes interference in some functions. All received messages on CAN are of standard type, so they are 11-bit identifiers.
Please guide me about setting the best mask filters due to the required IDs for this chip in the processor expert section.

Mizuz_0-1680860579382.png

receives messages with the following identifiers:

0x082 -> 0000 1000 0010

0x088 -> 0000 1000 1000

0x094 -> 0000 1001 0100

0x0A2 -> 0000 1010 0010

0x0AE -> 0000 1010 1110

0x0A9 -> 0000 1010 1001

0x0C2 -> 0000 1100 0010

0x0E9 -> 0000 1110 1001

0x0E8 -> 0000 1110 1000

0x0C9 -> 0000 1100 1001

0x028 -> 0000 0010 1000

0x109 -> 0001 0000 1001

0x129 -> 0001 0010 1001

0x149 -> 0001 0100 1001

0x169 -> 0001 0110 1001

0x189 -> 0001 1000 1001

0x150 -> 0001 0101 0000

0x749 -> 0111 0100 1001

0x70A -> 0111 0000 1010

0x288 -> 0010 1000 1000

0x62C -> 0110 0010 1100

0x68C -> 0110 1000 1100

0x6AC -> 0110 1010 1100

0 Kudos
Reply
0 Replies