AN1857 RS232 optoisolation interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN1857 RS232 optoisolation interface

1,091件の閲覧回数
edjiang
Contributor II

Hi,

 

I built a Hardware connection for MC9S08MP16, which is the same as described in app note AN1857, page 13. I try to communicate using Freemaster, with correct Baud rate setting. Unfortunately, it doesn't work. When I use P&E micro debugger, the communication is fine.

 

I measured my PC and found both pin 4 and pin 7 is of voltage around -11V. Anyone has an idea about this configuration?

 

Thanks

Ed

 

ラベル(1)
0 件の賞賛
7 返答(返信)

884件の閲覧回数
edjiang
Contributor II

forgot to mention that I use the "real" serial com port, NOT USB port.

0 件の賞賛

884件の閲覧回数
michaelsteffenf
NXP Employee
NXP Employee

Did you install the serial source code into your project?

Mike

0 件の賞賛

884件の閲覧回数
edjiang
Contributor II

Hi Mike,

that is the point. I don't know anything about the serial source code and I didn't find any information from the Freemaster webpage. Previously, I use P&E micro debugger, it works fine with Freemaster, which means my project code is okay. Now I need to communicate only using com port, that is the problem I have now.

Thanks

Ed

0 件の賞賛

884件の閲覧回数
bigmac
Specialist III

Hello Ed

For the optoisolated interface to work correctly when sending data to the PC, the signal at pin 7 (RTS) need to be set active by the PC, to achieve a voltage level of about +12 volts.  At the same time, the signal at pin 4 (DTR) should remain inactive, to retain the negative voltage level.

Regards,

Mac

0 件の賞賛

884件の閲覧回数
edjiang
Contributor II

Hi Mac,

Thanks for the explanation. Should I do anything about this voltage setting? or it is done automatically by Freemaster?

Ed

0 件の賞賛

884件の閲覧回数
michaelsteffenf
NXP Employee
NXP Employee

You need insert the serial driver files into the project if you’re going to communicate via serial connection. They are available on the Freescale web site in the Freemaster page.

Mike

0 件の賞賛

884件の閲覧回数
edjiang
Contributor II

Hi Mike,

Thanks for your reply. I didn't find the files on the webpage "FreeMASTER Run-Time Debugging Tool". Could you please send me the link to the files or a screenshot of the webpage?

Thanks

Ed

0 件の賞賛