A question regarding MC9S08JM32 usb module power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A question regarding MC9S08JM32 usb module power

1,245 Views
donperotti2
Contributor I

Hello, I'm making a testing board using the MC9S08JM32 for USB applications but I'm not sure i understand the power situation, according to the datasheet the USB-B connector should be routed like so:

dgsdgasasdg.png

However I've connected it like this:

gaewgdsg.png

In this design the VCC bar is either 3.3V or 5V depending on what source i connect to the board's power terminals.

P4 is a 3-pin strip intended to use a jumper between pins 1&2 or 2&3

The Vusb bar is connected to the MCU's VUSB33 pin.

This is an error right?

I'm not sure I understand what Vbus or what is supposed to connect to, does it come from the Host(PC)?

0 Kudos
Reply
1 Reply

1,125 Views
vicentegomez
NXP TechSupport
NXP TechSupport

PLease check

pastedImage_1.png

Internally the USBDP is tied to VUSB33 through a pull up

I hope this will help you

pastedImage_2.png

Regards

0 Kudos
Reply