9S08QG8 family 5V tolerant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S08QG8 family 5V tolerant

Jump to solution
1,964 Views
Cram
Contributor III

Hi all,

 

Does anybody knows if 9S08QG8 family are 5 V tolerant?
The low Vcc voltage (up to 3.6V) is just a matter of power consumption?

Thxs for any comment

Labels (1)
0 Kudos
1 Solution
639 Views
celsoken
Contributor V

Dear Cram,

 

Even if you homologate QG8 working on 5V, you'd be working outa specs.

When the next die shrink arrives, you could be in trouble.

Try the SH8, it's quite the same as Qg8, but it works on 5V, with higher pin count, low cost and and it is not hard to find.

 

Cheers,

 

Celso

View solution in original post

0 Kudos
5 Replies
639 Views
admin
Specialist II

Well I see you got an acceptable answer so I guess my reply is immaterial.

 

Anyway, I was going to say that I thought "5v tolerant" meant that the part was capable of accepting 5v levels on its inputs while operating at some other, lower voltage. But it appears you mean is it capable of actually operating at 5v.

 

If you run a QG at 3.3v and apply 5v to an input, it won't work. Something will have to give. There are substrate diodes from the I/O pins to the Vdd pin which would be forward biased if you did that.

0 Kudos
639 Views
peg
Senior Contributor IV

Hello,

 

For the record the absolute maximum for supply is 3.8 volts and for inputs is supply plus 0.3 volts. So under no circumstances can you apply 5 volts to the input

0 Kudos
640 Views
celsoken
Contributor V

Dear Cram,

 

Even if you homologate QG8 working on 5V, you'd be working outa specs.

When the next die shrink arrives, you could be in trouble.

Try the SH8, it's quite the same as Qg8, but it works on 5V, with higher pin count, low cost and and it is not hard to find.

 

Cheers,

 

Celso

0 Kudos
639 Views
Cram
Contributor III

Thx for all,

 

Yes I found the SH8 family after post the question, yes it pin to pin compatible with a little bit more options, but it will works!

 

Best rgards,

 

Cram

0 Kudos
639 Views
Superberti
Contributor I

I can confirm that this MCU is working without problems

on 4.0 V, but I did not test it with higher voltages.

 

Bye,

0 Kudos