68HC11A1 Replacement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

68HC11A1 Replacement

1,098 次查看
jimkustra
Contributor I

I am a design engineer recently tasked with support of a product that was designed several years ago (late 1990s) by a company that our company merged with. The product uses a Motorola MC68HC11A1CFNE3 (Motorola became Freescale and now NXP) that was discontinued around 2010 and no longer available. Our company had been purchasing the original part from brokers but stock is drying up. The Freescale notice has a recommended replacement as MC68HC11E1CFNE3 (still available) but not fully equivalent. In comparing the two devices, it appears the only difference is the size of the RAM was doubled from 256 Bytes to 512 Bytes. Since our company's original engineers are long gone and the source of the source code is questionable at this time, what are the chances that I can drop in the available part and program it with the present image used with the original part and run successfully?

0 项奖励
回复
1 回复

898 次查看
john_suchyta
NXP Employee
NXP Employee

Hi Jim,

The E1 is the replacement for the A1, but it takes a few changes to firmware and maybe hardware. Engineering Bulletin EB193 has the details. I don't believe you can just drop the A1 code into the E1.

Regards,

John Suchyta

0 项奖励
回复