Using the S08RN60 MCU for controlling a DC motor with Touch electrodes.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the S08RN60 MCU for controlling a DC motor with Touch electrodes.

Using the S08RN60 MCU for controlling a DC motor with Touch electrodes.

This example application implements Touch Sensing electrodes for controlling the enable, speed and direction of a DC motor. The RN60 is also controlling eight multiplexed 7-segments displays to indicate the percentage of speed.

The code was generated and compiled on CodeWarrior for Microcontrollers v10.6 and Processor Expert 10.3 for the Freescale HCS08 series of microcontrollers.

Labels (1)
Comments

The CodeWarrior v10.6 project is available at the following link:
Using the S08RN60 MCU for controlling a DC motor with Touch electrodes.

No ratings
Version history
Last update:
‎09-15-2014 02:20 PM
Updated by: