UM11829 TEA2017 SNSCAP参数疑惑

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UM11829 TEA2017 SNSCAP参数疑惑

Jump to solution
3,359 Views
LB_YJY
Contributor II

诸位好!    

    参考UM11829的参数做的项目,发现文档中的C13参数有疑惑,在参考设计的240W、150W和TTEA2017_Design_Tool 计算表格中,C13加C11的容量都不超过7nF,但是在UM11829文档中C13单个容量为10nF, 这个是不是大了点?C13+C11容量为16.8nF,个人感觉C13是不是为1nF?如图

 

0 Kudos
Reply
1 Solution
3,341 Views
guoweisun
NXP TechSupport
NXP TechSupport

C13可以先不用贴,留着位置空着先。

View solution in original post

0 Kudos
Reply
2 Replies
3,339 Views
LB_YJY
Contributor II

谢谢!顺便问下同样的参数在输出电压小于30V时,电流小于3A时,输出电压会有轻微纹波。在输出电压大于32V时,电流小到几百毫安都不会有纹波。也就是电容CR (c20)的波形不出现断续,输出就没有纹波。这个如何处理能否给点思路?

0 Kudos
Reply
3,342 Views
guoweisun
NXP TechSupport
NXP TechSupport

C13可以先不用贴,留着位置空着先。

0 Kudos
Reply