UM11829参数确认

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UM11829参数确认

2,015 Views
LB_YJY
Contributor II

新年好!

 UM11829文档中有几处确认

1 原理图中TF1 为1.5 mH,BOM清单中为15mH,这个应该以BOM为准吧?

2 原理图中C20 为22 nF,BOM清单中为22 nF,但是附带厂商料号为C822J104J60C000,这个料号为104电容,应该忽略这个厂商料号吧?

3 原理图中Q9的B E是连接在一起,能否简要说明工作原理?这里看不大明白如下图微信图片_20230130103141.png

4 能否回答下T1变压器 Lr 140uH Lm 820uH,是按照那种思路推倒出来的?我个人估计这两个参数是另外计算出来出结果,主要是实现宽电压范围输出。我自己在计算器表格中改变输入参数,是计算不出这样的结果。

刚刚入行,谢谢指导!

0 Kudos
Reply
2 Replies

1,992 Views
guoweisun
NXP TechSupport
NXP TechSupport

1 原理图中TF1 为1.5 mH,BOM清单中为15mH,这个应该以BOM为准吧?

[gw]你是对的BOM为准

2 原理图中C20 为22 nF,BOM清单中为22 nF,但是附带厂商料号为C822J104J60C000,这个料号为104电容,应该忽略这个厂商料号吧?

[gw]对的

3 原理图中Q9的B E是连接在一起,能否简要说明工作原理?这里看不大明白如下图

guoweisun_0-1675058291878.png

 

[ge]BE接到一起就是二极管了。

4 能否回答下T1变压器 Lr 140uH Lm 820uH,是按照那种思路推倒出来的?我个人估计这两个参数是另外计算出来出结果,主要是实现宽电压范围输出。我自己在计算器表格中改变输入参数,是计算不出这样的结果。

[gw]这是估算的例如  Estimated Magtizing inductor  tolerance (+/-) =7%

 

 

0 Kudos
Reply

1,989 Views
LB_YJY
Contributor II

非常感谢!

0 Kudos
Reply