TEA19161+19162异常保护

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA19161+19162异常保护

2,371 Views
bkl
Contributor I

@guoweisun 

你好!

使用TEA19161+19162设计的57V/500W电源,在负载为200W时,通电10分钟左右会自动断电,大约1.1s左右之后再启动,有时能重新启动,几分钟之后再次重启。有时是一直试图启动但总失败,间隔为1.1s左右。输出电压正常,排除OVP;刚开始通电的10分钟内能正常带载,输出电压/电流稳定,排除OPP。请帮忙分析下是OCP,OTP还是线圈磁饱和造成?或是提供下有效的检测方法。

谢谢!

0 Kudos
0 Replies