PCA9685每个LED驱动端口驱动电流能力问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9685每个LED驱动端口驱动电流能力问题

3,529 Views
yz_z
Contributor III

       请教一下NXP的技术支持工程师,PCA9685单个LED驱动端口的拉电流能力是多少?目前我要使用16路LED驱动端口,每个端口拉电流能力为1mA。我看该芯片手册上介绍说LED驱动端口是灌电流达到25mA,拉电流为10mA。但我不解的是这个介绍的是单个LED驱动端口,还是整个芯片16路LED驱动端口总共的灌电流达到25mA,拉电流10mA?

       望NXP技术支持工程师能给予解惑一下,谢谢。

0 Kudos
Reply
2 Replies

3,321 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个是单个口子的驱动能力,并不是全部的。

0 Kudos
Reply

3,321 Views
jinyuzhang
NXP Employee
NXP Employee

Hi 您好

     实在不好意思,这个社区只支持PF0100或者FS45、65等车载PMIC和Power SBC的产品,给您造成不便非常抱歉。请您联系SIP的AE或者FAE工程师来获取帮助

     谢谢!

BRs

jinyu

PMIC and SBC question
0 Kudos
Reply