FS8530

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,953 Views
Oliver2
Contributor III

你好,NXP团队。
我有几个关于FS8530的问题已经困扰了我几个星期了:
1.我在上电的时候给了WAKE1和VSUP=12V, DBUG=0V,启动后8530一直处于开启关断的循环,关断大约4S后重启,这似乎是challenge watchdog的问题。为了不断刷新watchdog, 我发现WD_SEED寄存器中默认的值0X5AB2通过Challenger watchdog formula计算后是0XA54D。0XA54D再次通过Challenger watchdog formula计算后又回到了0X5AB2,所以MCU要做的事是将0XA54D发送给WD_ANWSER后,再发送0XA54D给WD_SEED以此来刷新SEED,下一次刷新又是0X5AB2给WD_ANWER,再发送0X5AB2给WD_SEED,以此往复吗。不然我无法理解手册中对于刷新LFSR的SEED这一句话的理解。
2.手册中说在WINDOW OPEN的情况下发送WD_ANWSER才有用,那MCU如何判断是否在OPEN情况下呢。
3.我曾尝试关掉WD,我在给了DBUG=5V后,确实所有电压轨都关了,我利用SPI发送31000C35,想要在 OTP_CFG_BOOST_2寄存器里去关掉VBOOST,但是还是没用。

0 Kudos
1 Solution
1,688 Views
Oliver2
Contributor III

十分感谢,已经解决了

View solution in original post

0 Kudos
6 Replies
1,693 Views
guoweisun
NXP TechSupport
NXP TechSupport

这个问题解决了吗?

0 Kudos
1,689 Views
Oliver2
Contributor III

十分感谢,已经解决了

0 Kudos
1,683 Views
yangk
Contributor I

你好,怎么解决的?帮助一下

 

0 Kudos
1,673 Views
Oliver2
Contributor III

如果一直是我上述的4S重启这个问题的话,从状态机上看是你VMON的检测电压出了问题,所以ABIST1自检一直没通过。等VMON通过了后如果是看门狗的问题,出现的现象就是PGOOD不断的闪烁,然后又重启

0 Kudos
1,677 Views
guoweisun
NXP TechSupport
NXP TechSupport

如果有问题可以提交一个ticket:

Home (nxp.com)

0 Kudos
1,803 Views
yangk
Contributor I

你好。楼主,我遇到一样的情况。解决了吗?

0 Kudos