<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックFRDM-KW24D512 with raspberry pi</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW24D512-with-raspberry-pi/m-p/491188#M985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have made FRDM-KW24D512 work with iMX Ultralight linux board. The FRDM-KW24D512 was plugged in the Arduino connector in the iMXUl6 board and they work as Thread border gateway. Eveything works. &lt;/P&gt;&lt;P&gt;Now I want to make the FRDM-KW24D512 to work with raspberry pi. According to the documentation, the connection&lt;/P&gt;&lt;P&gt;between the FRDM-24D512 and any linux host need to be UART.&amp;nbsp; I have connect the UART of both. However&lt;/P&gt;&lt;P&gt;the firmware(thread_host_controller_device_imx6ulevk) ) in FDRM-25D512 is not running properly.&amp;nbsp; Should I connect some more wires between the FRDM-24D512 and the raspberry pi besides UART? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Mar 2016 18:09:45 GMT</pubDate>
    <dc:creator>waynezhao</dc:creator>
    <dc:date>2016-03-21T18:09:45Z</dc:date>
    <item>
      <title>FRDM-KW24D512 with raspberry pi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW24D512-with-raspberry-pi/m-p/491188#M985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have made FRDM-KW24D512 work with iMX Ultralight linux board. The FRDM-KW24D512 was plugged in the Arduino connector in the iMXUl6 board and they work as Thread border gateway. Eveything works. &lt;/P&gt;&lt;P&gt;Now I want to make the FRDM-KW24D512 to work with raspberry pi. According to the documentation, the connection&lt;/P&gt;&lt;P&gt;between the FRDM-24D512 and any linux host need to be UART.&amp;nbsp; I have connect the UART of both. However&lt;/P&gt;&lt;P&gt;the firmware(thread_host_controller_device_imx6ulevk) ) in FDRM-25D512 is not running properly.&amp;nbsp; Should I connect some more wires between the FRDM-24D512 and the raspberry pi besides UART? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Mar 2016 18:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW24D512-with-raspberry-pi/m-p/491188#M985</guid>
      <dc:creator>waynezhao</dc:creator>
      <dc:date>2016-03-21T18:09:45Z</dc:date>
    </item>
  </channel>
</rss>