<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K32W ISP mode in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077675#M9749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device can support up to 1M speed , the usage of the CTS and RTS are mostly used in application level and is up to the customers if they use it or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case the flash programmer can work without CTS and RTS, you can check more information about this in the Production Flash Programmer Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jun 2020 14:29:36 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2020-06-30T14:29:36Z</dc:date>
    <item>
      <title>K32W ISP mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077674#M9748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the SOC(Wifi module) is connected to K32W,&lt;/P&gt;&lt;P&gt;can Uart Rom Bootloader(ISP mode) run to 1M speed &lt;STRONG&gt;with no CTS/RTS&lt;/STRONG&gt; ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 10:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077674#M9748</guid>
      <dc:creator>danieltseng</dc:creator>
      <dc:date>2020-06-22T10:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: K32W ISP mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077675#M9749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device can support up to 1M speed , the usage of the CTS and RTS are mostly used in application level and is up to the customers if they use it or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case the flash programmer can work without CTS and RTS, you can check more information about this in the Production Flash Programmer Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2020 14:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077675#M9749</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-06-30T14:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: K32W ISP mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077676#M9750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Thank you for your reply, let me know that 1M uart speed can be achieved without CTS/RTS.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 02:05:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077676#M9750</guid>
      <dc:creator>danieltseng</dc:creator>
      <dc:date>2020-07-01T02:05:33Z</dc:date>
    </item>
    <item>
      <title>Re: K32W ISP mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077677#M9751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is good that this is clear now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 14:05:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W-ISP-mode/m-p/1077677#M9751</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-07-01T14:05:42Z</dc:date>
    </item>
  </channel>
</rss>