<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iBeacon + Connectable Peripheral with QN9080? in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/iBeacon-Connectable-Peripheral-with-QN9080/m-p/1069773#M9597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering if I can use the QN9080 as an iBeacon as well as a peripheral to connect to from an iPhone. I am able to get the iBeacon working with the Beacon demo in the SDK -- but now I want to also connect to the QN9080 for data transfer. Is this possible with one chip? Or do I need two?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 May 2020 07:31:07 GMT</pubDate>
    <dc:creator>mike6789</dc:creator>
    <dc:date>2020-05-11T07:31:07Z</dc:date>
    <item>
      <title>iBeacon + Connectable Peripheral with QN9080?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/iBeacon-Connectable-Peripheral-with-QN9080/m-p/1069773#M9597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering if I can use the QN9080 as an iBeacon as well as a peripheral to connect to from an iPhone. I am able to get the iBeacon working with the Beacon demo in the SDK -- but now I want to also connect to the QN9080 for data transfer. Is this possible with one chip? Or do I need two?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2020 07:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/iBeacon-Connectable-Peripheral-with-QN9080/m-p/1069773#M9597</guid>
      <dc:creator>mike6789</dc:creator>
      <dc:date>2020-05-11T07:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: iBeacon + Connectable Peripheral with QN9080?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/iBeacon-Connectable-Peripheral-with-QN9080/m-p/1069774#M9598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael, I hope you're doing well!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There's currently no implementation for a Beacon + Connectable peripheral on one device example available, but it could be a possible implementation. First a connection event should have to be triggered, then the device could keep sending non-connectable advertising packets.&lt;/P&gt;&lt;P&gt;For reference, could you please take a look at the BLE Application Developer's Guide, in the following path for the SDK?:&lt;/P&gt;&lt;P&gt;&amp;lt;…\SDK_2.2.2_QN908XCDK\docs\wireless\Bluetooth\Bluetooth Low Energy Application Developers Guide.pdf&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if you need any more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Take care, best regards,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 20:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/iBeacon-Connectable-Peripheral-with-QN9080/m-p/1069774#M9598</guid>
      <dc:creator>Sebastian_Del_Rio</dc:creator>
      <dc:date>2020-05-18T20:11:42Z</dc:date>
    </item>
  </channel>
</rss>