<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Use DBG_vPrintf() with IEEE 802.15.4 Application in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Use-DBG-vPrintf-with-IEEE-802-15-4-Application/m-p/1063720#M9530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The bug was in the makefile .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CFLAGS += -DDBG_ENABLED should come right after TRACE ?= 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That and I disabled&amp;nbsp; DEBUG ?= HW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2020 01:56:04 GMT</pubDate>
    <dc:creator>ramonet</dc:creator>
    <dc:date>2020-06-22T01:56:04Z</dc:date>
    <item>
      <title>Use DBG_vPrintf() with IEEE 802.15.4 Application</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Use-DBG-vPrintf-with-IEEE-802-15-4-Application/m-p/1063719#M9529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I simply trying to print into a terminal&amp;nbsp; using DBG_vPrint&amp;nbsp; I have tried so many combinations&lt;/P&gt;&lt;P&gt;but no matter what I cant get the uart to print into a terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a JN-5169 dongle with BeyondStudio.&lt;/P&gt;&lt;P&gt;And I modified the JN-AN-1174 template&amp;nbsp; (IEEE 802.15.4 Application Template for JN516x) end device file and makefile.&lt;/P&gt;&lt;P&gt;The files compile fine and the resulting bin can be loaded into the jn5169 dongle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached these modified files to this message.&lt;/P&gt;&lt;P&gt;I am doing the print call in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PUBLIC void AppColdStart(void)&lt;BR /&gt;{&lt;BR /&gt; /* Disable watchdog if enabled by default */&lt;BR /&gt; #ifdef WATCHDOG_ENABLED&lt;BR /&gt; vAHI_WatchdogStop();&lt;BR /&gt; #endif&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; vInitSystem();&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; DBG_vUartInit(DBG_E_UART_1, DBG_E_UART_BAUD_RATE_115200);&lt;/P&gt;&lt;P&gt;// vStartActiveScan();&lt;/P&gt;&lt;P&gt;while (1)&lt;BR /&gt; {&lt;BR /&gt; &lt;BR /&gt; DBG_vPrintf(TRUE,"Hello");&lt;BR /&gt; // vProcessEventQueues();&lt;/P&gt;&lt;P&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The issue must be something related to my makefile or am I using this UART function incorrectly?&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2020 08:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Use-DBG-vPrintf-with-IEEE-802-15-4-Application/m-p/1063719#M9529</guid>
      <dc:creator>ramonet</dc:creator>
      <dc:date>2020-06-18T08:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: Use DBG_vPrintf() with IEEE 802.15.4 Application</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Use-DBG-vPrintf-with-IEEE-802-15-4-Application/m-p/1063720#M9530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The bug was in the makefile .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CFLAGS += -DDBG_ENABLED should come right after TRACE ?= 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That and I disabled&amp;nbsp; DEBUG ?= HW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 01:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Use-DBG-vPrintf-with-IEEE-802-15-4-Application/m-p/1063720#M9530</guid>
      <dc:creator>ramonet</dc:creator>
      <dc:date>2020-06-22T01:56:04Z</dc:date>
    </item>
  </channel>
</rss>